The problem about shutdown or reboot on IMX6(DL/Q) with Android6.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem about shutdown or reboot on IMX6(DL/Q) with Android6.0.1

2,683 Views
pengxingwei
Contributor III

Hi all,

      I come cross a problem about shutdown or reboot, my board can't shutdown and reboot by using power button

the log as follows when I type the  reboot  command and the system is halt

   

root@sabresd_6dq:/ # reboot
sysrq: SysRq : Emergency Remount R/O
EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)
EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)
Emergency Remount complete
imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command ''
Reboot failed -- System halted

and when I enter the power button to power off ,as follow  ,the system is halting

About the problem above,How to solve it ?? Thanks

Labels (3)
0 Kudos
Reply
1 Reply

1,767 Views
joanxie
NXP TechSupport
NXP TechSupport

maybe you can refer to the link as below, hope helpful for you

https://community.nxp.com/thread/307212 

0 Kudos
Reply