The problem about register configuration of AR0234

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The problem about register configuration of AR0234

跳至解决方案
555 次查看
jax_wang
Contributor II

I am using AR0234 to learn driver develop, and now the sensor has alread to output 10bit image, but The 8-bits is not work successfully.

SO,

Do somebody know how to set the register of ar0234 to output 8bit raw image.
Thank you.

 

标记 (1)
0 项奖励
1 解答
516 次查看
jax_wang
Contributor II

Hi, khang_letruong

The key is register 0x3354, its value should be 0x2a, but the RR is show 0x32 for 8-bit.

在原帖中查看解决方案

0 项奖励
5 回复数
539 次查看
khang_letruong
Senior Contributor III

Hi @jax_wang ,

Register 0x31AC should be 0x0A08 (default is 0x0A0A)

Regards,
K.

0 项奖励
517 次查看
jax_wang
Contributor II

Hi, khang_letruong

The key is register 0x3354, its value should be 0x2a, but the RR is show 0x32 for 8-bit.

0 项奖励
529 次查看
jax_wang
Contributor II
Hi,Khang_letruong,
Firstly, thanks your reply.
I have changed the value of 0x31AC to 0x0A08, but it still occurs error. I message to you, could you help me check it?
Thank you.
0 项奖励
527 次查看
khang_letruong
Senior Contributor III

Hi @jax_wang ,

I shared you the description of the sensor's register relevant to 8/10-bit Bayer output. You might also need full datasheet from vendor for checking other registers as well.

Regards,

K

0 项奖励
542 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you need to know how to configure AR0234 camera to support 8bits, you need consult from Onsemi, if you use it on the imx8mp board, current bsp supports this format already

0 项奖励