The operating range of i.MX8M-Mini USB1_VBUS/USB2_VBUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The operating range of i.MX8M-Mini USB1_VBUS/USB2_VBUS

Jump to solution
2,212 Views
james_wu
Contributor IV

According to the i.MX8M-Mini Datasheet, the operating range of USB1_VBUS and USB2_VBUS is from 0.8V to 3.6V.
And the absolute maximum rating is 3.95V.

But the voltage level of USB1_VBUS and USB2_VBUS on the i.MX8M-Mini EVK Base Board is still 5V.

pastedImage_3.png

Any impact or side effect if we use 5V on USB1_VBUS/USB2_VBUS for a long term usage?

Labels (1)
1 Solution
2,024 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

on i.MX8M Mini EVK schematic (SPF-31399) processor USBn_VBUS is connected

through R108/109 30K. According to Table 11-76. External Signals i.MX8MMini Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MMRM.pdf

The PHY VBUS0 pin must not connect directly to the 5v VBUS voltage
on the USB2.0 link. The PHY VBUS0 pin must be isolated by an external resistor
(REXT1) so that the PHY VBUS0 pin sees a lower voltage.

Design Tool
i.MX 8M Mini Evaluation Kit Design Files
i.MX 8M Mini Evaluation Kit | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,025 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

on i.MX8M Mini EVK schematic (SPF-31399) processor USBn_VBUS is connected

through R108/109 30K. According to Table 11-76. External Signals i.MX8MMini Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MMRM.pdf

The PHY VBUS0 pin must not connect directly to the 5v VBUS voltage
on the USB2.0 link. The PHY VBUS0 pin must be isolated by an external resistor
(REXT1) so that the PHY VBUS0 pin sees a lower voltage.

Design Tool
i.MX 8M Mini Evaluation Kit Design Files
i.MX 8M Mini Evaluation Kit | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------