The network performance of MX6 GbE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The network performance of MX6 GbE

ソリューションへジャンプ
3,348件の閲覧回数
george
Senior Contributor II

Dear all,

We designed the original board which used i.MX6 and KSZ9031RNX (Micrell GbE-PHY).

However, in the transfer rate using iperf, it is 300-400Mbps.

Are these values appropriate?

Are there any data about the network performance of MX6 GbE?

Best Regards,

George

ラベル(7)
0 件の賞賛
返信
1 解決策
2,524件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Please take a look at the following errata document:

http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Errata: ERR004512.

Let me know if you have additional questions.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,522件の閲覧回数
EricNelson
Senior Contributor II

Hi George,

We have some notes about i.MX6 Gb ethernet and the variables involved in this blog post:

     http://boundarydevices.com/i-mx6-ethernet/

2,524件の閲覧回数
george
Senior Contributor II

Dear Eric

Thank you.

I am glad to see the real measurement report of those other than us.

Best Regards,

George

0 件の賞賛
返信
2,525件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Please take a look at the following errata document:

http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Errata: ERR004512.

Let me know if you have additional questions.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,524件の閲覧回数
george
Senior Contributor II

Dear Sergio,

Thanks.

However, I do not know why it needs to be indicated in Errata documet.

I think that it is not Errata of Device.

Don't you think so?

Best Regards,

George

0 件の賞賛
返信