The mipi output problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The mipi output problem

1,974 Views
pingyuchen
Contributor II

Hi,

Now  I use the imx8mq evk board to test the mipi output. I use boot-imx8mq-mipi-panel.img and can measure the mipi signal when the board is booted. But I find the mipi signal isn't output when the board is resumed from the suspend mode by ON/OFF button. Where can I modify to fix this problem?

Best Regards,

0 Kudos
Reply
4 Replies

1,815 Views
igorpadykov
NXP Employee
NXP Employee

Hi pingyu

this issue is described in Table 13. Known issues and workarounds for i.MX 8MQuad

attached Release Notes.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,815 Views
pingyuchen
Contributor II

Hi Igor,

Thank you for your response. By the way, is there a scheduler for the new release? And can this issue be solved in the new release if we need the system suspending and resuming?

0 Kudos
Reply

1,815 Views
igorpadykov
NXP Employee
NXP Employee

Hi pingyu

one can try attached patch and Linux L4.9.123

linux-imx - i.MX Linux kernel 

Best regards
igor

0 Kudos
Reply

1,814 Views
pingyuchen
Contributor II

Hi igor,

I used the patch and this issue is fixed.

Thank you very much!

0 Kudos
Reply