The mfgToolLib.dll in L4.9.11_1.0.0-ga_mfg-tools will cause mfgtool can't detect device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The mfgToolLib.dll in L4.9.11_1.0.0-ga_mfg-tools will cause mfgtool can't detect device.

1,304 Views
leima
Contributor III

Os: win10

mfgtool version: L4.9.11_1.0.0-ga

When try to use this version mfgtool to load uboot.bin, I found that it can't detect my imx6q board until I replaced the mfgToolLib.dll file with the "L4.1.15_2.0.0-ga" version one.

Is there anybody has the same problem?

Labels (1)
Tags (1)
0 Kudos
3 Replies

879 Views
KazuhisaTaira
Contributor IV

I face same problem. It was locale setting of Windows 10.

If system locale is not English, please try to change English.

I used this tool, it is OK.

Releases · xupefei/Locale-Emulator · GitHub 

879 Views
joanxie
NXP TechSupport
NXP TechSupport

what media and OS do you use? emmc or sd card? linux or android? and which .vbs file do you use? give me your detailed test steps,let me reproduce this on my board.

0 Kudos

879 Views
leima
Contributor III

PC OS: win10

imx6q Os: yocto linux

Both emmc and sd card.

This is a custom board using imx6q soc, so I run "MfgTool2.exe" and just use it to burn the uboot.bin to the spi flash.

I thought that there is matter with the configure files like "cfg.ini", "ucl2.xml" or emmc, sd card, this is the problem detecting the usb device.

0 Kudos