Os: win10
mfgtool version: L4.9.11_1.0.0-ga
When try to use this version mfgtool to load uboot.bin, I found that it can't detect my imx6q board until I replaced the mfgToolLib.dll file with the "L4.1.15_2.0.0-ga" version one.
Is there anybody has the same problem?
I face same problem. It was locale setting of Windows 10.
If system locale is not English, please try to change English.
I used this tool, it is OK.
what media and OS do you use? emmc or sd card? linux or android? and which .vbs file do you use? give me your detailed test steps,let me reproduce this on my board.
PC OS: win10
imx6q Os: yocto linux
Both emmc and sd card.
This is a custom board using imx6q soc, so I run "MfgTool2.exe" and just use it to burn the uboot.bin to the spi flash.
I thought that there is matter with the configure files like "cfg.ini", "ucl2.xml" or emmc, sd card, this is the problem detecting the usb device.