The lowest frequence of i.MX8M Mini in high temperature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The lowest frequence of i.MX8M Mini in high temperature

641 次查看
jimmyli
Contributor IV

Hi,

      We take the i.MX8M Mini (MIMX8MM6DVTLZAA, commercial level) to run in full speed (1.8GHz), while the environment is 35℃ constantly.  When the i.MX8M Mini chip temperature is high than 95℃ (read register), the chip will power down, and then the frequency is 1.2GHz which I know is the lowest value.

      My question: what is the lowest frequence of i.MX8M Mini can be set in high temperature? 

      We need the i.MX8M Mini to slow down to drop down the temperature, rather than power down.

      Thanks.

标签 (1)
0 项奖励
2 回复数

638 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jimmy

 

>My question: what is the lowest frequence of i.MX8M Mini can be set in high temperature? 

 

from hardware point of view there is no limitation. From software, one can look at imx8mm.dtsi,

a53_opp_table: opp-table, thermal-zones

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mm.dtsi?...

and sect.2.5.3 CPU Frequency Scaling (CPUFREQ), sect.2.9 Thermal   i.MX Linux Reference Manual​

 

Best regards
igor

0 项奖励

630 次查看
jimmyli
Contributor IV

Hi Igor,

      Thanks for your reply.

      We will check it again.

0 项奖励