@shanashiro
Hello,
It depends on applications - using external pulling resistors.
Note, i.MX6ULL pins state during reset (except Boot Mode Configuration
Pins) are not specified.
Customers can use use Table 91 (14 x 14 mm Functional Contact Assignments),
column"Out of Reset Condition"
https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf
Also
https://community.nxp.com/t5/i-MX-Processors/about-pin-mode-during-POR-on-i-MX6ULL/m-p/1153519
Regards,
Yuri.
GPIO is not pin/PAD(IOMUX).
GPIO only has data register, which is logic "0", or "1".
GPIO, ADC and SAI are equal.
Please check for the pad/pin Out of Reset Condition in datasheet.
During the reset, it is hi-z.