The level of GPIO on reset state in i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The level of GPIO on reset state in i.MX6ULL

449 Views
shanashiro
Contributor I
Is it need pull up or pul down GPIO on reset state in i.MX6ULL?
0 Kudos
2 Replies

440 Views
Yuri
NXP Employee
NXP Employee

@shanashiro 
Hello,

  It depends on applications - using external pulling resistors. 
Note, i.MX6ULL pins state during reset (except Boot Mode Configuration
Pins) are not specified. 

  Customers can use use Table 91 (14 x 14 mm Functional Contact Assignments),
column"Out of Reset Condition"

https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf

  Also

https://community.nxp.com/t5/i-MX-Processors/about-pin-mode-during-POR-on-i-MX6ULL/m-p/1153519

Regards,
Yuri.

0 Kudos

441 Views
BiyongSUN
NXP Employee
NXP Employee

GPIO is not pin/PAD(IOMUX).

 

GPIO only has data register, which is logic "0", or "1". 

GPIO, ADC and SAI are equal. 

Untitled.png

Please check for the pad/pin Out of Reset Condition in datasheet.

During the reset, it is hi-z.

 

Untitled2.png

 

 

0 Kudos