The i.MX7D which pin can use SRAM external memory?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The i.MX7D which pin can use SRAM external memory?

跳至解决方案
1,179 次查看
felixhsu
Contributor III

Hi All

As title, my customer want to use SRAM(pure SRAM, not PSRAM) on i.MX7D,

Please tell me SRAM can use which pin connect to i.MX7D.

Thanks.

标签 (1)
0 项奖励
回复
1 解答
1,046 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Felix

one can use EIM interface for connection to SRAM, the same as

using parallel nor-flash, may be useful to look at application note

http://www.cypress.com/file/202616/download 

http://www.cypress.com/file/207256/download 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,047 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Felix

one can use EIM interface for connection to SRAM, the same as

using parallel nor-flash, may be useful to look at application note

http://www.cypress.com/file/202616/download 

http://www.cypress.com/file/207256/download 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复