The i.MX7D which pin can use SRAM external memory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The i.MX7D which pin can use SRAM external memory?

ソリューションへジャンプ
1,258件の閲覧回数
felixhsu
Contributor III

Hi All

As title, my customer want to use SRAM(pure SRAM, not PSRAM) on i.MX7D,

Please tell me SRAM can use which pin connect to i.MX7D.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,125件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

one can use EIM interface for connection to SRAM, the same as

using parallel nor-flash, may be useful to look at application note

http://www.cypress.com/file/202616/download 

http://www.cypress.com/file/207256/download 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,126件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

one can use EIM interface for connection to SRAM, the same as

using parallel nor-flash, may be useful to look at application note

http://www.cypress.com/file/202616/download 

http://www.cypress.com/file/207256/download 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信