The gaid line of camera is not continuous.---->CSI setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The gaid line of camera is not continuous.---->CSI setting

1,624件の閲覧回数
xiaoying_lu
Contributor III

The customer is complaimed that the gaid line of camera is not continuous.

The camera pathway is: CVBS--->Tcon IC--->BT656-4 output--->i.MX6 IPU block.

Now original setting of CSI is blow. This setting that the gaid line of camera is not continuous.

IPU2_CSI1_CCIR_CODE_1:0x000D07DF

IPU2_CSI1_CCIR_CODE_2:0x00040596

Then change the setting of CSI , the gaid line will be continuous.

IPU2_CSI1_CCIR_CODE_2:0x00040584

The detail of this problem is discribed in the file of "i.MX6_CSI setting_Camera GaidLine is not continuous.xlsx".

We want to know the operating principle of this change.

ラベル(1)
0 件の賞賛
返信
1 返信

1,502件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

   I  will reply you on the link: https://community.nxp.com/thread/509684 

So the ticket will be closed.

BR,

Weidong

0 件の賞賛
返信