The function of SNVS_LPCR register in i.MX6SX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The function of SNVS_LPCR register in i.MX6SX

ソリューションへジャンプ
838件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Please tell me the following registers function.

pastedImage_4.png

I want to control power ON/OFF by SW in i.MX6SX.

I understand it can power off by DP_EN and TOP fields from following thread.

i.MX6 SNVS_LPCR register and power down 

However, I can't understand how to power on by SW.

 

According to the RM, it seems that it can be power on by PK_OVERRIDE or PK_EN.

Can user power on by those bit ?

Also could you tell me the function of PK_OVERRIDE and PK_EN ?

Ko-hey

ラベル(4)
0 件の賞賛
返信
1 解決策
714件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

For i.MX6SX  SNVS[PK_OVERRIDE],  SNVS[PK_EN] are not supported

there is internal ticket get the RM updated accordingly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
715件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

For i.MX6SX  SNVS[PK_OVERRIDE],  SNVS[PK_EN] are not supported

there is internal ticket get the RM updated accordingly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信