The condition when measured i.MX6 power net electrical performance.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The condition when measured i.MX6 power net electrical performance.

跳至解决方案
1,380 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6 layout.

Please see chapter 3.17 in IMX6DQ6SDLHDG Rev.1, 65 mohm or less @ 100MHz is recommended.

However, our partner felt the value is too small if it was measured on the edge of pad of the board that parts are mounted.

So would you let me know the condition when it was measured and where was measured point?

(e.g. no parts are mounted, measured point is center of a pad, same power rail pad of parts are shorted.)

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (1)
0 项奖励
回复
1 解答
1,270 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Satoshi Shimoda,

You are correct, this data is simulated by HyperLynx from Mentor Graphic.

"Open-circuit" means only bare PCB is simulated and no any loading is added.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,270 次查看
satoshishimoda
Senior Contributor I

Hi community,

I understood it is simulation data and the condition is "open-circuit" from IMX6DQ6SDLHDG Rev.1.

Then, I want to confirm the meaning of "open-circuit" in this case.

i.MX6 is not mounted? or other load parts are not mounted also?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,271 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Satoshi Shimoda,

You are correct, this data is simulated by HyperLynx from Mentor Graphic.

"Open-circuit" means only bare PCB is simulated and no any loading is added.

0 项奖励
回复