The condition to enter i.MX6SDL Wakeup From Low Power Mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The condition to enter i.MX6SDL Wakeup From Low Power Mode.

Jump to solution
653 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL boot.

Please see Figure 8-1 in IMX6SDLRM, I want to know the condition to enter "Wakeup From Low Power Mode".

Would you let me know it?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
568 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

condition : if PGC_CPU_SR=1, then enter "Wakeup From Low Power Mode".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
569 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

condition : if PGC_CPU_SR=1, then enter "Wakeup From Low Power Mode".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos