The captured image is black when debuging the tw9990

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The captured image is black when debuging the tw9990

1,029件の閲覧回数
tangyuan
Contributor III

HI: 

    I am debuging the tw9990. Tw9990 is PAL/NTSC to BT656.I use mxc_v4l2_tvin.c to test tw9990 and the captured image is black.It is the log information.

  ty.PNG

  Can you anyone help me .

ラベル(5)
0 件の賞賛
返信
1 返信

755件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

IPU_INT_STAT_5=0x00000001 means a lot, I couldn't tell root issue from this warning, but I send the link as below to you for reference,

https://community.nxp.com/thread/322841 

0 件の賞賛
返信
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----