The captured image from OV5640 has a lot of lines

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The captured image from OV5640 has a lot of lines

969件の閲覧回数
liamtien
Contributor I

OV5640 connects to i.MX6Q through DVP, the captured image has a lot of lines.

Its captured image is similar to https://www.programering.com/q/MTNyAjNwATY.html

I guess this is caused by noise, but does the frequency drift of pixel clock also bring up noise? 

If this is a hardware issue, then how to fix it? Thanks. 

ラベル(2)
0 件の賞賛
返信
1 返信

910件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello liam,

If software is the same noise can be from hardware, please check analog supplies and its noise, sensor cables.

Attach sensor from good board to custom and check if that helps. One can try to test with imx-test (folder mxc_v4l2_test) in

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

also one can check signals with oscilloscope and using app note

http://www.analog.com/media/en/technical-documentation/application-notes/AN-1337.pdf 

 

Regards

0 件の賞賛
返信