The cameras on the SABRE board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The cameras on the SABRE board

Jump to solution
1,219 Views
patcharasirigul
Contributor II

Hello everyone,

I bought the SABRE board coming with the camera like a picture below. I would like to know what the part number of the camera using on the Sabre board is ? or where can I find the camera same this module ?

IMG_1722[1].JPG.jpg

IMG_1721[1].JPG.jpg

thank you so much,

Patchara Sirigulyanon

Labels (2)
0 Kudos
1 Solution
621 Views
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

part numbers are given on link below

Camera modules for i.MX6 Quad SABRE Smart Device Platform (Ref.MCIMX6Q-SDP)

many vendors can offer these modules, for example

www.a-kerr.com.

www.nuhorizons.com

Best regards

igor
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
622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

part numbers are given on link below

Camera modules for i.MX6 Quad SABRE Smart Device Platform (Ref.MCIMX6Q-SDP)

many vendors can offer these modules, for example

www.a-kerr.com.

www.nuhorizons.com

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos