The cameras on the SABRE board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The cameras on the SABRE board

ソリューションへジャンプ
1,218件の閲覧回数
patcharasirigul
Contributor II

Hello everyone,

I bought the SABRE board coming with the camera like a picture below. I would like to know what the part number of the camera using on the Sabre board is ? or where can I find the camera same this module ?

IMG_1722[1].JPG.jpg

IMG_1721[1].JPG.jpg

thank you so much,

Patchara Sirigulyanon

ラベル(2)
0 件の賞賛
1 解決策
620件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

part numbers are given on link below

Camera modules for i.MX6 Quad SABRE Smart Device Platform (Ref.MCIMX6Q-SDP)

many vendors can offer these modules, for example

www.a-kerr.com.

www.nuhorizons.com

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
621件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

part numbers are given on link below

Camera modules for i.MX6 Quad SABRE Smart Device Platform (Ref.MCIMX6Q-SDP)

many vendors can offer these modules, for example

www.a-kerr.com.

www.nuhorizons.com

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛