The adapted platform is i.MX6Q , the current status is in routing stage , we will have the PDN simulation ,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The adapted platform is i.MX6Q , the current status is in routing stage , we will have the PDN simulation ,

1,295 Views
canerchu
Contributor I

The adapted  platform is i.MX6Q ,  the current status is in routing stage , we will have the PDN simulation ,

please help to release the i.MX6Q PDN spec for our simulation .

Labels (1)
0 Kudos
Reply
3 Replies

1,154 Views
igorpadykov
NXP Employee
NXP Employee

Hi caner

available simulation models are release at link below

"Simulation and Models"

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

I am afraid power integrity simulation models are not available.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,154 Views
canerchu
Contributor I

Hi Igor ,

after checking the FSL website of "Simulation and Models" ,

ibis had implemented by ourself ,

but we are also lack with the PDN spec for the judgement of the PDN

simulation ,

If or not , all of FSL platforms are without this simulation , (it is

relative the performance of system design ) ;

Have any solution for this PDN simulation review ?

Best Regards

Caner Chu 邱忠正

**************************************

華冠通訊股份有限公司

產品研發本部 硬體研發二處 硬體設計三部

Arima Communications Corp

23586 新北市中和區中正路866號6樓

6F , No.866 Zhong Zheng Rd. , Zhong He Dist. , New Taipei City , 23586 ,

Taiwan (ROC)

Tel : 02-8227-7755 ext : 3546

Fax : 02-8227-5533

Email : canerchu@arimacomm.com.tw

**************************************

igorpadykov <admin@community.freescale.com>

2015/04/07 上午 09:15

請回信 給

jive-911472886-502g-2-ar3z@freescale.hosted.jivesoftware.com

收件人

caner chu <canerchu@arimacomm.com.tw>

副本抄送

主旨

Re: - The adapted platform is i.MX6Q , the current status

is in routing stage , we will have the PDN simulation ,

The adapted platform is i.MX6Q , the current status is in routing stage ,

we will have the PDN simulation ,

reply from igorpadykov in i.MX Community - View the full discussion

Hi caner

available simulation models are release at link below

"Simulation and Models"

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

I am afraid power integrity simulation models are not available.

Best regards

igor

0 Kudos
Reply

1,154 Views
igorpadykov
NXP Employee
NXP Employee

Hi caner

suggest to follow power design recommendartions given in

IMX6DQ6SDLHDG

Best regards

igor

0 Kudos
Reply