The access method to PCIE_RC_BAR0 register.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The access method to PCIE_RC_BAR0 register.

Jump to solution
1,020 Views
george
Senior Contributor II

Dear All,

We have planned the product which used i.MX6DL.

And, The product works PCIe on RTOS.

We are investigating how to use PCIe and are investigating the access method to PCI-Configuration space now.

In " i. MX 6Solo/6 DualLite Applications Processor Reference Manual, Rev.1, and 04/2013 ",

PCIE_RC_BAR0 register modification is described to be "Bits[3:0] are writable through the DBI."

Please tell me the PCIE_RC_BAR0 register modification method via DBI.

* I cannot find the materials about it.

Best Regards,

George

Labels (6)
0 Kudos
Reply
1 Solution
814 Views
b47504
NXP Employee
NXP Employee

In RC side, you should be able to modify the register directly. As you know, for CDM space,  you can modify some of them through local bus, or by the remote partner through pcie wire. 

View solution in original post

0 Kudos
Reply
2 Replies
815 Views
b47504
NXP Employee
NXP Employee

In RC side, you should be able to modify the register directly. As you know, for CDM space,  you can modify some of them through local bus, or by the remote partner through pcie wire. 

0 Kudos
Reply
814 Views
george
Senior Contributor II

Dear Yuan,

Thanks.

0 Kudos
Reply