Hi All.
As you may know, the maximum supported resolution of VP8 codec is 1280x720.
The i.MX6 datasheet shows the following:
![MX6_VPU_Spec.png MX6_VPU_Spec.png](/t5/image/serverpage/image-id/30250iADABCD3D9D822AA3/image-size/large?v=v2&px=999)
However, as a result of testing with several files(MKV, WebM), the VP8 codec with 1920x1080 resoltuion was also supported.
I tested video decoding using VPU on android 7.1 and Windows Embedded Compact 2013(WEC 2013) OS.
Use the VPU instead of SW type VP8 codec.
I hope this information will help you.
Have a nice day.