The USB not recognized

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The USB not recognized

2,074 次查看
937556508
Contributor I

Hi,

We use the MIMX8MM5DVTLZAA chip to carry the circuit design. Now the USB1 interface used to download the image is not recognized. Can you help me?

We are designing with reference to the USB2 circuit of the 8MMINILPD4-EVK development board. The following figure has additional circuit diagrams alarge.pngUSB不识别.PNGnd unidentified signs. and the PIN of USB1_ID is NC.

0 项奖励
回复
3 回复数

2,070 次查看
937556508
Contributor I

I'm very sorry that my description looks a bit confusing, let me reorganize it.

 

We use the MIMX8MM5DVTLZAA chip to carry the circuit design. Now the USB1 interface used to download the image is not recognized. Can you help me?

We are designing with reference to the USB2 circuit of the 8MMINILPD4-EVK development board. The following figure has additional circuit diagrams and unidentified signs. and the PIN of USB1_ID is NC.

Best regards.

0 项奖励
回复

2,059 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 937556508

 

one can recheck usb connections using checklist in

i.MX 8M Mini Hardware Developer’s Guide

try to test it for example in linux, booting from  sd or emmc. For preparing boot

image try sect.4.3.2 Copying the full SD card image i.MX Linux User’s Guide​

 

Best regards
igor

0 项奖励
回复

2,046 次查看
937556508
Contributor I

Hi igor

Thank you very much for your reply.

I checked my circuit and think it is ok.

My board only has emmc boot, and there is no emmc card slot, so I have no way to download the boot image to emmc in advance.

Do you have other ways to help me?

In addition, I use the USB-type-C interface, is it a type-c problem?

Looking forward to your help.

 

Best regards

0 项奖励
回复