The SRTC power consumption and a LiCELL battery life

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The SRTC power consumption and a LiCELL battery life

1,154 Views
george
Senior Contributor II

Dear all,

We use i.MX6 with MMPF0100 for our product.

When an external power supply is not connected, it is described in the datasheet that SRTC-block current consumption is 41uA.

=> Page 30 : http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

For example, when we refer to SDP and use the Li-Cell battery(Panasonic : ML621 - 5mA/h) for RTC, it can keep up RTC only for 122 hours.

* 5mA / 41uA ≒ 121.9hour (≒5.08days)

If this is true, we need to change into the battery of larger capacity.

Is there any way of reducing "41uA" keeping up RTC?

Best Regards,

George

Labels (1)
0 Kudos
Reply
3 Replies

819 Views
Yuri
NXP Employee
NXP Employee

  As for RTC current in SNVS Only mode, the following is footnote for the table in the Datasheet :

"The typical values shown here are for information only and are not guaranteed.

These values are average values measured on a worst-case wafer at 25 C."

So, real values may be less or greater, and - alas - we do not have app note
how to decrease consumption.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

819 Views
george
Senior Contributor II

Dear Yuri,

Thank you for the quick response.

Are "41uA" Worst-case wafer?

The datasheet of the link which I indicate is described to be typical-case wafer.

=> Page 30 : http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Please let me know one.

Are 41uA the cases where X'tal is used?

Or is it the case where a ring oscillator is used?

=> Section 4.5.2 / Page 37 : http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best Regards,

George

0 Kudos
Reply

819 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.
> Are "41uA" Worst-case wafer?


41 uA is not maximum, in this sense it is not the worst case.

2.

> Are 41uA the cases where X'tal is used?


Yes.

~Yuri.

0 Kudos
Reply