The Power Consumption for i.MX6 Quad PLUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Power Consumption for i.MX6 Quad PLUS

ソリューションへジャンプ
2,693件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We use i.MX6Quad now.
We want to use i.MX6Quad PLUS next.


We want to confirm power consumption for i.MX6Quad PLUS.

(We want to compare Quad PLUS with Quad)
However, we were not able to find this in a Web site.


May I have a power consumption application notes for i.MX6Quad PLUS?

Best Regards,
Yuuki

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,769件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yuuki,

There is not an Application Note covering Power Consumption for the i.MX6QP yet, but the recommendation is to use the Application Note for the i:MX6Q as reference in the meantime.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Power Consumption for the i.MX6QP is expected to be higher than the i.MX6Q but not by much. The PF0100 should suit the i.MX6QP needs after the specs were updated for SW2 from 2A to 2.5A.

I hope this information helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,770件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yuuki,

There is not an Application Note covering Power Consumption for the i.MX6QP yet, but the recommendation is to use the Application Note for the i:MX6Q as reference in the meantime.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Power Consumption for the i.MX6QP is expected to be higher than the i.MX6Q but not by much. The PF0100 should suit the i.MX6QP needs after the specs were updated for SW2 from 2A to 2.5A.

I hope this information helps!

Regards,

0 件の賞賛
返信