The PCIE suspend issue in IMX8 series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The PCIE suspend issue in IMX8 series

ソリューションへジャンプ
1,138件の閲覧回数
charleshuang
Senior Contributor II

Hello NXP 

Refer the community, i.MX8M Quad EVK board the suspend /resume function is fail in PCIE interface.

https://community.nxp.com/t5/i-MX-Processors/i-mx8-PCIe-Wi-Fi-Suspend-Resume-Fails/m-p/1219849

About the imx8 all series (imx8mm imx8mp imx8qxp ), it is the same issue about suspend fail.

Right ?  

ラベル(1)
0 件の賞賛
返信
1 解決策
1,118件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @charleshuang ,

I hope you are doing well.

We have tested suspend/resumed functions of the imx8mm-evk board with the QCA9377 Wi-Fi chipset successfully.
there has been no issue with suspending and resuming the PCIe interface on imx8m boards.

Thanks & Regards

Sanket Parekh

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,119件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @charleshuang ,

I hope you are doing well.

We have tested suspend/resumed functions of the imx8mm-evk board with the QCA9377 Wi-Fi chipset successfully.
there has been no issue with suspending and resuming the PCIe interface on imx8m boards.

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信