The Camera Image is Split.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The Camera Image is Split.

跳至解决方案
2,005 次查看
donggyulee
Contributor I

Hi All,

I'm testing the camera of i.mx6 demo kit.

(The Board is SabreSD 6Q)

The camera image is not good.

The Camera image was split in two.

Please Check the attached file.

My System :

     Linux 3.0.101

     Camera Module : OV5640 Mipi

     Test command :  ./unit_tests/mxc_v4l2_overlay.out -iw 1920 -ih 1080 -ow 1920 -oh 1080 -di /dev/video1

Please advise.

Thank you

0 项奖励
回复
1 解答
1,834 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

seems driver does not cover the 1080p 30fps option and although it’s theoretically possible

to achieve, it would require the coefficient  pair values to tweak the frame rate. These coefficient

tables are given by Omnivision. One can use drivers provided for other boards, like Sabre Lite board.

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.10.17_1.0.0_ga/drivers/media/platf...

Alternatively one may look for other 3rd party efforts:

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,835 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DongGyu

seems driver does not cover the 1080p 30fps option and although it’s theoretically possible

to achieve, it would require the coefficient  pair values to tweak the frame rate. These coefficient

tables are given by Omnivision. One can use drivers provided for other boards, like Sabre Lite board.

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.10.17_1.0.0_ga/drivers/media/platf...

Alternatively one may look for other 3rd party efforts:

http://dl.linux-sunxi.org/SDK/A23-v1.0/unpacked/A23/lichee/linux-3.4/drivers/media/video/sunxi-vfe/d...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,834 次查看
donggyulee
Contributor I

Hi igor

Thank you so much

You are a nice guy:smileyhappy:

0 项奖励
回复