The CSI setting of IPU-----i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The CSI setting of IPU-----i.MX6

1,170 Views
xiaoying_lu
Contributor III

The customer is complaimed that the gaid line of camera is not continuous.

 

The camera pathway is: CVBS--->Tcon IC--->BT656-4 output--->i.MX6 IPU block.

 

 

Now original setting of CSI is blow. This setting that the gaid line of camera is not continuous.

 

IPU2_CSI1_CCIR_CODE_1:0x000D07DF

 

IPU2_CSI1_CCIR_CODE_2:0x00040596

 

 

Then change the setting of CSI , the gaid line will be continuous.

 

IPU2_CSI1_CCIR_CODE_2:0x00040584

 

The detail of this problem is discribed in the file of "i.MX6_CSI setting_Camera GaidLine is not continuous.xlsx".

 

 

We want to know the operating principle of this change.

Labels (1)
Tags (1)
0 Kudos
1 Reply

999 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Xiaoyin,

   

I consulted i.MX expert on this question. See his reply:

------------------------

Customer should not change the CCIR_CODE_1 and CCIR_CODE_2 setting if the input is standard BT656.

Customer can check the IPU_CSI_OUT_FRM_CTRL register setting, CSI_VSC = 2 or 3, it will get different result in memory.

------------------------

Hope the answer can help you !

BR,

weidong

0 Kudos