The CSI setting of IPU-----i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The CSI setting of IPU-----i.MX6

1,964 次查看
xiaoying_lu
Contributor III

The customer is complaimed that the gaid line of camera is not continuous.

 

The camera pathway is: CVBS--->Tcon IC--->BT656-4 output--->i.MX6 IPU block.

 

 

Now original setting of CSI is blow. This setting that the gaid line of camera is not continuous.

 

IPU2_CSI1_CCIR_CODE_1:0x000D07DF

 

IPU2_CSI1_CCIR_CODE_2:0x00040596

 

 

Then change the setting of CSI , the gaid line will be continuous.

 

IPU2_CSI1_CCIR_CODE_2:0x00040584

 

The detail of this problem is discribed in the file of "i.MX6_CSI setting_Camera GaidLine is not continuous.xlsx".

 

 

We want to know the operating principle of this change.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,793 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Xiaoyin,

   

I consulted i.MX expert on this question. See his reply:

------------------------

Customer should not change the CCIR_CODE_1 and CCIR_CODE_2 setting if the input is standard BT656.

Customer can check the IPU_CSI_OUT_FRM_CTRL register setting, CSI_VSC = 2 or 3, it will get different result in memory.

------------------------

Hope the answer can help you !

BR,

weidong

0 项奖励
回复