Test secure boot without locking the e-fuse

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Test secure boot without locking the e-fuse

1,867 次查看
Hardevsinh_Palaniya
Contributor III

Processor : i.MX8M mini
OS : Yocto Zeus
u-boot : u-boot-2020.04
Kernel : 5.4.47

Hi,
I am implementing secure boot on i.MX8M mini and completed all configurations with High Assurance Boot (HAB) and compilation done. I would like to test it on a test board  without writing e-fuse permanently.

Is it possible to test secure boot (with HAB) without locking e-fuse?  How can i do that? can you give me any related docs?

Any help will be appreciated.

Senior Embedded Engineer | hardevsinh.palaniya@siliconsignals.io | www.siliconsignals.io
0 项奖励
回复
2 回复数

1,839 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Hardevsinh_Palaniya 

No, We can't test secure boot without programming fuse.  But We don't need to close device.

Best regards

Harvey

 

0 项奖励
回复

1,836 次查看
Hardevsinh_Palaniya
Contributor III

Hi @Harvey021 
Thanks for your reply.
I know that I can not test secure boot without programming fuse.  According to the https://community.nxp.com/t5/i-MX-Processors/eFUSE-Question/m-p/511419/highlight/true#M83385 ,  I can't revert the fuse once I write 1 to the fuse bit. If it is so, there is a chance of losing one hardware.
Is there any possibility of reversing the fuse after testing?

Senior Embedded Engineer | hardevsinh.palaniya@siliconsignals.io | www.siliconsignals.io
0 项奖励
回复