Temperature monitor of IMX6UL doesn't work as expected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temperature monitor of IMX6UL doesn't work as expected

1,051 Views
jeffreylee
Contributor I

I have the same issue, please e-mail the patch to me, thanks

0 Kudos
Reply
2 Replies

926 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You the patch.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

926 Views
matthewdahl
Contributor I

I am working on two imx6 based boards that are experiencing this incorrect display of temperature. 

Is this patch only available through email? If no where if yes can you forward it my way.

Thanks,

0 Kudos
Reply