Temperature monitor of IMX6UL doesn't work as expected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature monitor of IMX6UL doesn't work as expected

ソリューションへジャンプ
4,688件の閲覧回数
ethanyang
Contributor II

We now have the use of i.MX6UL on our products.

According to the Security Reference Manual, low-temperature monitor should assert between -40 and -20 degree.

However we found that some units will start to have the temperature tamper event at -16 degree C.

We've tried the TEMP_LOW_OFFSET bits of DryIce Tamper Offset Control Register (SNVS Expanded_DTOCR), but it makes no different.

And there's another issue about the temperature shown by u-boot.

The CPU temperature is abnormal when the unit is placed in a chamber with temperature below 0 C.

u-boot_temp.png

Not sure if the behavior of temperature monitor is related to the wrong temperature.

But it'll be helpful if there is a fix for this.

Thanks.

Ethan

ラベル(1)
1 解決策
3,905件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 The BSP does not support negative temperature value.

I've sent patch to try via e-mail.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
3,905件の閲覧回数
registry_chou
Contributor I

Hi Yuri,

Our engineering team has a question for this, but Ethan has leave for a long time.

Could you provide the patch for us? And we need try to reach -35 C.

Regards,

Jeff

0 件の賞賛
返信
3,905件の閲覧回数
Yuri
NXP Employee
NXP Employee

registry.chou@gmail.com 

Hello,

  Please create separate request or thread

Support | NXP 

Regards,

Yuri.

0 件の賞賛
返信
3,905件の閲覧回数
registry_chou
Contributor I

Okay.

0 件の賞賛
返信
3,905件の閲覧回数
ethanyang
Contributor II

Hi Yuri,

Thanks for the information.

Any chance that we can lower the asserting range by configuring some register?

And what about the wrong temperature display in u-boot? Do you know if there is a fix for it?

Regards,

Ethan

0 件の賞賛
返信
3,905件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

1.

   I sent You some comments regarding the temperature monitor directly via e-mail.

2.

  On my i.MX6 UL EVK :

 

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:27:03 -0500)

CPU: Freescale i.MX6UL rev1.0 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 36C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
MMC: no card present
Net: FEC1
Normal Boot
Hit any key to stop autoboot: 0
=>

Regards,

Yuri.

0 件の賞賛
返信
3,905件の閲覧回数
ethanyang
Contributor II

Hi Yuri,

1. Sorry I didn't mentioned that, but we're already using the trim value.

2. The issue we found is that u-boot shows wrong a negative temperature. No problem in showing a positive temerature.

Regards,

Ethan

0 件の賞賛
返信
3,906件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 The BSP does not support negative temperature value.

I've sent patch to try via e-mail.

Regards,

Yuri.

0 件の賞賛
返信
3,859件の閲覧回数
sunzhg20
Contributor II

Can you provide me with the patch pack?

0 件の賞賛
返信
3,853件の閲覧回数
Yuri
NXP Employee
NXP Employee

@sunzhg20 

Hello,

 

   Please create new request / thread regarding the issue.

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 件の賞賛
返信
3,881件の閲覧回数
sunzhg20
Contributor II

我也遇到这个问题 IMX6ULL 温度出现负数

这个如何打补丁?谢谢!

0 件の賞賛
返信
3,905件の閲覧回数
ethanyang
Contributor II

Hi Yuri,

The patch works. Thanks a lot.

Regards,

Ethan

3,905件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  have You tried to check general system operation under the low temperature, using,

say, DDR stress test ?

i.MX6/7 DDR Stress Test Tool V2.60 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信
3,905件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  Accuracy of the temperature sensor is not very high (+/-5 degree) .

Also, please look at app note AN5215 (i.MX 6 Temperature Sensor Module)

http://www.nxp.com/assets/documents/data/en/application-notes/AN5215.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信