Target frequency of the core for i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Target frequency of the core for i.MX6DL

ソリューションへジャンプ
1,448件の閲覧回数
yuuki
Senior Contributor II

Dear all,

The following is explained about Target frequency of the core in Reference Manual.

IMX6SDLRM Rev. 2, 04/2015
 1.4 Features (P.204)
====================================================================================
Target frequency of the core (including Neon and L1 cache) is 800 MHz non-overdrive
over the specified temperature range:
 . 1 GHz overdrive over the specified temperature range
 . 800 MHz non-overdrive over the specified temperature range
====================================================================================

Does MCIMX6U5EVM10** correspond to overdrive?

I think that this description is related only to MCIMX6U7CVM08**(Speed Grade: 800MHz).

May I have advice?

Best Regards,

Yuuki

ラベル(2)
0 件の賞賛
返信
1 解決策
1,185件の閲覧回数
art
NXP Employee
NXP Employee

Actually, the Consumer grade parts (MCIMX6U5xxx and MCIMX6U8xxx) are specified for 1GHz core operation to increase the system performance, whereas the Industrial grade parts (MCIMX6U7xxx), that require more reliability, are only specified for 800MHz core operation. Of course, the MCIMX6U7xxx parts can also run at 1GHz core clock frequency, but in that case the reliability and lifetime parameters, declared for Industrial grade parts, cannot be guaranteed.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,186件の閲覧回数
art
NXP Employee
NXP Employee

Actually, the Consumer grade parts (MCIMX6U5xxx and MCIMX6U8xxx) are specified for 1GHz core operation to increase the system performance, whereas the Industrial grade parts (MCIMX6U7xxx), that require more reliability, are only specified for 800MHz core operation. Of course, the MCIMX6U7xxx parts can also run at 1GHz core clock frequency, but in that case the reliability and lifetime parameters, declared for Industrial grade parts, cannot be guaranteed.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信