Hi,
We are using imx6ul G3 in our of our custom design. We want to configure TAMPER_PIN 9 as GPIO but we are unable to do so.
We tried to set the SW_MUX_CTL_PAD_SNVS_TAMPER9 SW MUX Control Register (0x020E0040) to value 0x5 but when we read back its showing as 0. We tried the same with all the other TAMPER pins(0-9) as well. Also, when we read the fuse register(0x430, TAMPER_PIN_DISABLE[1:0]), its giving value as 0xf0216801 ( Which means TAMPER_PIN_DISABLE[1:0] is set to 0x2(10)).
Please let us know how to configure Tamper Pin as GPIO’s .
Regards,
vineeth
The TAMPER_DISABLE_PIN[1:0] = 2 means the Tamper pins 2, 3, 4, 7, 8, 9 are configured to function as the tamper pins so you cannot use them as GPIO pins.
Hello,
Tamper pins can function as GPIO, depending on TAMPER_PIN_DISABLE[1:0] fuse settings.
Say, for the i.MX6UL G2, the fuses TAMPER_PIN_DISABLE[1:0] = 11, meaning TAMPER0-9 used as GPIO.
But in i.MX6UL G3 release the tamper pins cannot be used as GPIO.
Can't disable tamper pins on imx6ul G3
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!