I am using i.MX6UL SoC with my custom hardware . I have built yocto with "DISTRO : fsl-imx-fb" , now I am running my QT application with 7 inch touch screen LCD interfaced to it.
Now it is required to take my QT application remotely and interacted from my remote client. Kindly requesting you for the suggestions on what packages need to add in my yocto to achieve this.
Yocto version : Yocto Zeus. I dont want to use x11.
@jimmychan, thanks for the reply .
As mentioned above , I am using Yocto version - 3.0 (zeus) , kernel version - 5.4-r0 .
Now my requirement is to take my QT application remotely and interacted from my remote client . For this I need your suggestions/procedure on what packages need to add in my yocto to achieve this.
I dont want to use x11..
Thanks
We have different version of BSP that the kernel is L5.4.xx. Please select one of them to use and build.
>> "QT application remotely and interacted from my remote client . ".
We don't have similar QT example. For the QT application example, I would suggest you to consult the QT forum or find the example in Google.
e.g. https://community.teamviewer.com/English/kb/articles/109833-grab-remote-screen-for-qt-applications