TX6Q LCD pwm-backlight: "probe of backlight failed with error -22"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TX6Q LCD pwm-backlight: "probe of backlight failed with error -22"

943 次查看
J_W
Contributor III

Hi,

I'm trying to activate an LCD display but the backlight won't turn on - actually /sys/class/backlight is empty. I assume that it is a device tree problem?

 

device tree:

 

aliases {
    backlight: backlight {
		compatible = "pwm-backlight";
		pwms = <&pwm2 0 500000 PWM_POLARITY_INVERTED>;
		power-supply = <&reg_lcd1_pwr>;
		/*
		 * a poor man's way to create a 1:1 relationship between
		 * the PWM value and the actual duty cycle
		 */
		brightness-levels = < 0  1  2  3  4  5  6  7  8  9
				     10 11 12 13 14 15 16 17 18 19
				     20 21 22 23 24 25 26 27 28 29
				     30 31 32 33 34 35 36 37 38 39
				     40 41 42 43 44 45 46 47 48 49
				     50 51 52 53 54 55 56 57 58 59
				     60 61 62 63 64 65 66 67 68 69
				     70 71 72 73 74 75 76 77 78 79
				     80 81 82 83 84 85 86 87 88 89
				     90 91 92 93 94 95 96 97 98 99
				    100>;
		default-brightness-level = <50>;
	};

 

 

dits:

 

aliases {
		pwm0 = &pwm1;
		pwm1 = &pwm2;

 

 

 

pinctrl_pwm2: pwm2grp {
		fsl,pins = <
			MX6QDL_PAD_GPIO_1__PWM2_OUT		0x1b0b1
		>;
	};
&pwm2 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_pwm2>;
	#pwm-cells = <3>;
	status = "okay";
};
pwm2: pwm@02084000 {
				#pwm-cells = <2>;
				compatible = "fsl,imx6q-pwm", "fsl,imx27-pwm";
				reg = <0x02084000 0x4000>;
				interrupts = <0 84 IRQ_TYPE_LEVEL_HIGH>;
				clocks = <&clks IMX6QDL_CLK_IPG>,
					 <&clks IMX6QDL_CLK_PWM2>;
				clock-names = "ipg", "per";
				status = "disabled";
			};

 

Also tried with status = "okay" on the last bit of code but it doesn't change anything.

Appreciate any help. Thanks!

0 项奖励
回复
0 回复数