TP2850 de-interlace driver for iMX8MP boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TP2850 de-interlace driver for iMX8MP boards

4,463 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se  and @joanxie ,

After referring to the website you provided, there will be a problem that mx8_v4l2_cap_drm_64 cannot be recorded, please help analyze this issue, thank you.

 

Here is my environment:

HW platform: IMX8MP

Video-In: TP2850

Linux Version: 5.10.52

Android Version: 11

 

Refer to your previous article on de-interlace:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...

 

1. Refer to the Patch provided by your article (L5.4.0_2.3.0_ISL7998x_Patch.7z)

FredTsai_1-1664780450642.png

 

2. After unzip, I refer to 0001-ISI-Add-de-interlace-support.patch to Patch to my BSP

FredTsai_2-1664780665860.png

 

3. DTS isi_0 settings are as follows (NTSC weave mode):

FredTsai_0-1664851936446.png

 

 

4. After applying PATCH, use mx8_v4l2_cap_drm_64 to verify, the result cannot be recorded, it will always stop at (v4l2_device_streamon:1478): channel[0] v4l_dev=0x4 start capturing.

(command: mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 1280 -oh 720 –of)

 

5. The attached file is the LOG of the video recorded by mx8_v4l2_cap_drm_64, and the ISI0 register has been dumped.

 

Please help to analyze this issue, thank you.

 

Thanks

Fred

0 Kudos
32 Replies

3,116 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Since you are using PAL camera, the command line should be:

mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 720 -oh 576 –of

ISI can't do sw-interlace and scaling together. And If you are using Android, you should run the unit test application in storage card folder.

0 Kudos

3,084 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

The resolution has been changed to 720x576, the command as follows:
mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 720 -oh 576 -of

But the situation is the same, still can't record video

Thanks
Fred

0 Kudos

3,043 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

For 720x576 PAL camera, register  "CHNL_IMG_CFG[0x0c]: 1e002d0" should be 0x012002d0.

0 Kudos

3,079 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

If your camera is 720x576, in ISI register, it should set to this resolution too. 

but from your ISI register dump: "CHNL_IMG_CFG[0x0c]: 1e002d0", it is 720x480.

0 Kudos

2,965 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

Tested with mx8_v4l2_cap_drm_64, after setting 720*576, the CHNL_IMG_CFG reg is still 720*480, and the result is correct when using other resolutions.
Does BSP support this resolution? how to fix this issue?

 

mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 720 -oh 576 -of
CHNL_IMG_CFG[0x0c]: 1e002d0  (720*480)

mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 640 -oh 480 -of
CHNL_IMG_CFG[0x0c]: 1e00280  (640*480)

mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 720 -oh 480 -of
CHNL_IMG_CFG[0x0c]: 1e002d0  (720*480)

mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 1280 -oh 1440 -of
CHNL_IMG_CFG[0x0c]: 2d00500  (1280*720)

mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 1920 -oh 1080 -of
CHNL_IMG_CFG[0x0c]: 4380780  (1920*1080)

 

Thanks
Fred

0 Kudos

2,961 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The resolution is reported from your TP2850 driver then set into ISI register, so you should check what's the resolution reported from your TP2850 driver, and is there any hard coding that you had modified in ISI code.

0 Kudos

2,955 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

I hardcoded the resolution in TP2850, set width = 720, height = 288,
After setting:
mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 720 -oh 576 -of

Results is correct:
CHNL_IMG_CFG[0x0c]: 12002d0

But there is still a stuck problem, unable to record video.
The attached file is the test LOG.

 

Thanks
Fred

0 Kudos

2,949 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

If your driver can work with normal camera mode, 720x288@60fps, then without any change in TP2850 and application, just updated the ISI registers to de-interlace mode setting and set de-interlace to DISP_MIX_GASKET_0_CTRL, then de-interlace can work. 

 

I don't have any more comments on this topic. 

0 Kudos

2,927 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

The result is as follows:

1.
non add nxp interlaced patch tp2850 reg set progressive mode 720x576: (non_nxp_patch.log)

FredTsai_0-1669341511882.png

2.
add nxp interlaced patch tp2850 reg set progressive mode 720x576  (add_nxp_patch.log)

FredTsai_1-1669341620373.png

 

3.
add nxp interlaced patch tp2850 set reg interlced pal mode 720x576 (add_nxp_patch_pal.log)

FredTsai_2-1669341726258.png

 

Thanks
Fred

0 Kudos

2,923 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

You don't need change the TP2850 mode, it should always work in interlaced PAL mode, and iMX8MP side can use different mode to capture it. 

Case 1: For TP2850 PAL output, if there is Frame end and Frame start in two fields, then iMX8 side can capture it as 720*288@50 fps without de-interlace.

Case 2: For TP2850 PAL output, if there os no Frame end and Frame start in two fields, then iMX8 side can capture it as 720*576@25 fps without de-interlace. 

 

After the above case works, then you can enable the iMX8 ISI de-interlace. For all these testing, TP2850 should always output same interlace PAL signals. If you use different TP2850 setting for test, that is no meaning.

And you need check with TP2850 side, is there Frame End and Frame Start bwtween two interlaces fields? 

0 Kudos

2,735 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

And you need check with TP2850 side, is there Frame End and Frame Start bwtween two interlaces fields?
According to TP2850 SPEC, it has Frame End and Frame Start, which is being confirmed with TP2850 vendor.

1.
From the observation of OV5640 driver, the PAL NTSC resolution defined by OV5640 Driver is correct, why the PATCH you provided is 1280*1440 instead of 1280*720 (720i), and the recorded video is not 1280*720, but 1280 *1440.
Record video with the following command:
mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 1280 -oh 1440 -of
The recorded video link is as follows:
https://drive.google.com/file/d/10ChIU77RoYyuqr3qfp_edWnqlQCI15Rv/view?usp=sharing

2.
Observing the PATCH provided by you, the register of the OV5640 is not changed, so can the OV5640 be set as an interlace output?
If this is ok, can I use 720*480 to verify de-interlace?
command:
mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video1" -fmt YUYV -ow 720 -oh 480 -of

3.
TP2850 Setting:
3-1 TP2850 Pixel PCLK calculation method: 2360 x 525/ 2 x 60 = 37.170 MHz (H-Total Pixel= 2360, line = 525/2, frame rate = 60Hz (not deinterlace yet))

3-2 Active needs to be changed to 1980 x 480, H-active becomes 1980 because it needs to correspond to H-total, normal H-total changes from 858 to 2360, multiplied by 2.75 times, so Active = 720x2.75 = 1980

3-3 Compare OV5640 PATCH, add TEST_MODE_1980_960 related code

3-4 The MIPI signal output by TP2850 is 60 pictures per second, and the SoC needs to do deinterlace to change it to 30 pictures

3-5 Not connected to NTSC input, directly output blue screen, blue screen (MIPI OUTPUT) is also output for the above settings

 

4.
Test Command: mx8_v4l2_cap_drm_64 -cam 1 -d "/dev/video0" -fmt YUYV -ow 1980 -oh 960 -of

CHNL_IMG_CFG[0x0c]: 1e007bc
STS( Channel Status Register (CHNL_STS) ) = 0x60020100
Please help to analyze why EARLY_VSYNC_ERR?

Thanks
Fred

0 Kudos

3,159 Views
TerryBarnaby1
Contributor IV

We are using a TP2856 on a custom IMX8MP platform. We were told that the IMX8MP's ISI was relatively crippled and did not support de-interlacing and so we implemented a software de-interlacer gstreamer module.

Is it actually true that we could use the ISI to de-interlace a PAL CSI2 video stream ?

 

0 Kudos

3,374 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

What's the camera's input resolution? If it is 1280*720, it should a progressive signal, no de-interlace is needed. 

If it is not 1280*720, then in ISI, you must set the same resolution as the camera original resolution, de-interlace can't work with scaling or CSC.

0 Kudos

3,367 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

 

Input resolution: CVBS (NTSC de-interlace)

 

The attached file is the LOG of the video recorded by mx8_v4l2_cap_drm_64, and the ISI0 CSI register has been dumped, resolution set to 720*480.

it will always stop at (v4l2_device_streamon:1478): channel[0] v4l_dev=0x4 start capturing.

 

Please help to analyze this issue, thank you.

 

Thanks

Fred

0 Kudos

3,332 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

From "CSIS_INTSRC[14]: 0x00000010", there is no MIPI FRAME_START and FRAME_END bits appear, that means no valid MIPI packages received. 

For different camera sensor, the "csis-hs-settle" value in device tree should be adjusted basded on MIPI CSI2 data rate.

 

And before debug the de-interlace mode, you need make sure the normal camera capture works first. If there are no FE(Frame End) and FS(Frame Start) between the two fields, then software can capture it as a normal 720*480@30fps camera. Two fields will be captured in to one buffer.

If there are FE and FS between the two fields, then software can capture it as a normal 720*240@60fps camera.

When no de-interlace mode works, then you can debug the de-interlace mode.

 

0 Kudos

3,317 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

1. Through oscilloscope measurement, TP2850 has MIPI signal output, as shown in the figure below.

MIPI Clock

FredTsai_1-1666070400249.png

MIPI Data

FredTsai_0-1666070383905.png

 

2. Below is the tp2850 mipi csi DTS setting. 
    When the TP2850 is set to progressive and remove de-interlaced patch, capture works.

FredTsai_3-1666070828995.png

 

3. Make sure the normal camera capture works first.
    (Use mx8_v4l2_cap_drm_64 to verify the OV5640 camera)

FredTsai_2-1666070568062.png

 

Do you have any suggestions for DEBUG?

 

Thanks

Fred

0 Kudos

3,313 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

For iMX8MP de-interlace, imx8-mipi-csi2-sam.c should be updated for de-interlace, this is different to iMX8QXP.

diff --git a/drivers/staging/media/imx/imx8-mipi-csi2-sam.c b/drivers/staging/media/imx/imx8-mipi-csi2-sam.c
index 1d12365520a6..ddfe30fb2a0a 100644
--- a/drivers/staging/media/imx/imx8-mipi-csi2-sam.c
+++ b/drivers/staging/media/imx/imx8-mipi-csi2-sam.c
@@ -228,6 +228,9 @@

/* display_mix_clk_en_csr */
#define DISP_MIX_GASKET_0_CTRL 0x00
+#define GASKET_0_CTRL_INTERLACE_MODE(x) (((x) & (0x3)) << 6)
+#define GASKET_0_CTRL_INTERLACE_MODE_MASK ((0x3UL) << (6))
+
#define GASKET_0_CTRL_DATA_TYPE(x) (((x) & (0x3F)) <<
#define GASKET_0_CTRL_DATA_TYPE_MASK ((0x3FUL) << (8))

@@ -988,6 +991,13 @@ static void disp_mix_gasket_config(struct csi_state *state)
if (fmt_val == GASKET_0_CTRL_DATA_TYPE_YUV422_8)
val |= GASKET_0_CTRL_DUAL_COMP_ENABLE;
val |= GASKET_0_CTRL_DATA_TYPE(fmt_val);
+
+ val &= ~GASKET_0_CTRL_INTERLACE_MODE_MASK;
+
+ printk("%s, field interlaced=%d\n", __func__, (state->format.field == V4L2_FIELD_INTERLACED? 1 : 0));
+ if (state->format.field == V4L2_FIELD_INTERLACED)
+ val |= GASKET_0_CTRL_INTERLACE_MODE(0x2);
+
regmap_write(gasket, DISP_MIX_GASKET_0_CTRL, val);

if (WARN_ON(!mf->width || !mf->height))
--

0 Kudos

3,309 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

After adding the patch to the BSP, the situation is the same, the attachment is Failed LOG, I have added LOG for DEBUG.

Thanks

Fred

0 Kudos

3,298 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The verified working patch is attached, we used the ov5640 camera for test, and handle its frame (1280*720) as field, then after de-interlace, the capture frame is 1280*1440.

You can reference to it and identify is there any difference. By the way, to debug the driver, I think you'd better use the unit test application "mx8_v4l2_cap_drm.out" first. 

0 Kudos

3,272 Views
FredTsai
Contributor I

Hi @qiang_li-mpu_se ,

The attached file is the LOG and recorded video of OV5640 and TP2850.

Removed L5.4.0_2.3.0_ISL7998x_Patch.7z, use
0001-Add-ISI-weaving-deinterlace-support-for-i.MX8MP.patch,
The result can be recorded to video through mx8_v4l2_cap_drm,
It should be correct to output a blue picture, but currently only see a blue line.

FredTsai_0-1666337168089.png

 

DTS:

FredTsai_1-1666337202461.png

FredTsai_2-1666337220308.png

Please analyze or provide suggestions, thank you.

 

Thanks
Fred

0 Kudos