TLV320AIC3104-Q1: Need to understand the dynamic switching between two different codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TLV320AIC3104-Q1: Need to understand the dynamic switching between two different codec

594 Views
divyeshmarne0
Contributor III

Hi Team,

Need your help to understand the dynamic switching between two different codec.

We are using:

  1. TLV320AIC3110 - Internal Audio Codec - 0.8W
  2. TLV320AIC3104-Q1 -External Audio Codec (20W*2 Speakers)

So basically we are confused between switching in two codec.

Both the codecs having their own significance.

Could you please suggest any idea to switch between the codecs dynamically.

For example:

if I'm connecting my mobile to Android Device which is having Audio codec thru BT, and I want to play audio from  TLV320AIC3104 External Audio Codec, then what need to be done?

 

thanks.

Divyesh

0 Kudos
2 Replies

580 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos

509 Views
divyeshmarne0
Contributor III

This link is for driver porting. Not helpful.

0 Kudos