TEE logs are not available in DMESG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEE logs are not available in DMESG

693件の閲覧回数
rnamburi
Contributor I

I am unable to see TEE logs in dmesg even after increasing the loglevel with 

 CFG_TEE_CORE_LOG_LEVEL=4
 CFG_TEE_TA_LOG_LEVEL = 4

 

Could please let me know, where am i missing.

0 件の賞賛
返信
8 返答(返信)

408件の閲覧回数
rnamburi
Contributor I
Did you build ATF image with optee enabled?
how to check this?
 
Please check Linux Kernel dmesg information, can you get "optee" related information?
this is the optee related information from dmesg.:
Line 104: [    0.000000] L2C-310 optee cache controller enabled try to unlock
Line 244: [    0.768908] optee soc:firmware:optee: probing for conduit method from DT.
Line 245: [    0.769082] optee soc:firmware:optee: teetz outer mutex: ret=0 pa=0x8fa00000 va=0xf0376000
Line 246: [    0.769558] optee soc:firmware:optee: initialized driver
 
0 件の賞賛
返信

404件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

If you configure the following settings, you will get OPTEE related information in atf(u-boot) log.

 CFG_TEE_CORE_LOG_LEVEL=4
 CFG_TEE_TA_LOG_LEVEL = 4

If no, it seems that you didn't build atf image with optee enabled.

You need to build atf images with option "SPD=opteed BL32=<optee_binary>" enabled.

In addition, you need to perform TA operation, then you will get related log in dmesg.

0 件の賞賛
返信

650件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I usually set the above two configurations, and when U-boot starts, I can see the Optee message.
First, confirm if the message can be seen in u-boot(atf) console log.

0 件の賞賛
返信

632件の閲覧回数
rnamburi
Contributor I
i could not see config parameters in u-boot logs. i have enabled them in yacto build. But how to check those configs are enabled in target after flashing?
0 件の賞賛
返信

571件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

$ bitbake optee-os -c cleansstate

$ bitbake imx-atf -c cleansstate

$ bitbake imx-boot -c cleansstate

$ bitbake optee-os -c patch

Go to  folder build-xwayland/tmp/work/imx8mpevk-poky-linux/optee-os/4.6.0.imx/git, please modify mk/config.mk according to your debug level setting.

$ bitbake optee-os

$ bitbake imx-atf

$ bitbake imx-boot

Then check optee message in your Kernel console log.

0 件の賞賛
返信

456件の閲覧回数
rnamburi
Contributor I

i have made the changes in mk/config.mk

I am not using yacto recipe for hartos compilation. Instead i use following commands to generate hartos image. 

echo "<------------Building Hartos-------------------->"

echo "<============Exporting Toolchain Path and setting enviornment Variable=============>"
export CROSS_COMPILE=arm-elina-linux-gnueabi-
export ARCH=arm
export PLATFORM=imx
export COMPILE_NS_USER=32
LDFLAGS=

echo "<==========Compiling Hartos ==========>"
make clean
make all

after flashing the hartos image. i dont see any TA applicatoin logs in dmesg.

do you any suggestions on this?

0 件の賞賛
返信

427件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Did you build ATF image with optee enabled?

Please check Linux Kernel dmesg information, can you get "optee" related information?

0 件の賞賛
返信

400件の閲覧回数
rnamburi
Contributor I

Did you build ATF image with optee enabled?

Yes

Please check Linux Kernel dmesg information, can you get "optee" related information?

these are the optee traces from dmesg
Line  53: [    0.000000] L2C-310 optee cache controller enabled try to unlock
Line 193: [    0.769007] optee soc:firmware:optee: probing for conduit method from DT.
Line 194: [    0.769177] optee soc:firmware:optee: teetz outer mutex: ret=0 pa=0x8fa00000 va=0xf0376000
Line 195: [    0.769652] optee soc:firmware:optee: initialized driver
Line 350: [    1.590184] systemd[1]: Started tee-supplicant Service.
Line 738: [   12.083898] BT_DOMAIN_ID  KPI MARKER: 12s070912666ns CON_Bt_sendGcfMsg_BSS_GAP_SetBTStateEnable
0 件の賞賛
返信