System stuck at "Starting kernel" by booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System stuck at "Starting kernel" by booting

1,274 Views
yaolinchang
Contributor I

Hi All,

         Sometimes we add new device driver or modify present files.

However the system will stuck at "Starting kernel" when we boot board.

How do we check or debug this situation?

Some sample log as below:

==================================

U-Boot 2014.04 (Mar 20 2015 - 23:54:26)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 24 C, calibration data: 0x5864ce7d

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

mmc1 is current device

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

5564616 bytes read in 271 ms (19.6 MiB/s)

Booting from mmc ...

reading imx6q-sabresd.dtb

42195 bytes read in 19 ms (2.1 MiB/s)

Kernel image @ 0x12000000 [ 0x000000 - 0x54e8c8 ]

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800d4d2

switch to ldo_bypass mode!

Starting kernel ...

Thanks,

Best Regards,

Yao

Labels (1)
0 Kudos
Reply
4 Replies

1,008 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which Board and BSP are you using?

0 Kudos
Reply

1,008 Views
yaolinchang
Contributor I

iMX6Q

0 Kudos
Reply

1,008 Views
jimmychan
NXP TechSupport
NXP TechSupport

so, make sure you are building the images for i.MX6Q SabreSD board.

What files you change or add? Basically, the DDR working proper and debug Uart setting correct, the kernel should be boot up and the debug message output from the debug uart .

0 Kudos
Reply

1,008 Views
yaolinchang
Contributor I

i.MAX 6 Series SABRE fpr Smart Devices

0 Kudos
Reply