System no response while  print out VPU blocking: timeout and rcu_sched_state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System no response while  print out VPU blocking: timeout and rcu_sched_state

2,657 Views
fdact
Contributor I

I was play mp4 file, then a period of time found that there was no reaction to the system.This phenomenon is the probability of occurrence that need to play video a long time . I will upload the log . Can you give some advice?

 

 

Thanks.

Original Attachment has been moved to: systen_hang_up_paly_mp4.log.zip

Labels (1)
0 Kudos
Reply
9 Replies

2,395 Views
igorpadykov
NXP Employee
NXP Employee

this is kernel error, also android is based on linux.

~igor

0 Kudos
Reply

2,395 Views
igorpadykov
NXP Employee
NXP Employee

do you see red in my previous post from 05.06.2016 21:29

1.jpg

click on red with mouse.

0 Kudos
Reply

2,395 Views
fdact
Contributor I

HI igor,

    Our board uses android OS, but the document is for ubuntu OS.

0 Kudos
Reply

2,393 Views
igorpadykov
NXP Employee
NXP Employee

please refer to attached file

igor

0 Kudos
Reply

2,393 Views
fdact
Contributor I

Hi igorpadykon,

    I didn't find any attached file.

0 Kudos
Reply

2,393 Views
igorpadykov
NXP Employee
NXP Employee

Hi ferdinand

seems you are using L3.0.35 with gpu lib 4.6.9, this is very old,

suggest to upgrade at least to L3.0.101_4.1.1 as it fixed many gpu bugs:

Board Support Packages (38)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite

Linux BSP Source Code Files (REV L3.0.101_4.1.1.)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,393 Views
fdact
Contributor I

Hi igorpadykon,

    Now the problem is still not resolved, you have any way?

0 Kudos
Reply

2,393 Views
fdact
Contributor I

Hi igorpadykov,

   Files IMX_MMCODEC_3.0.101_4.1.1_Bundle.tar.gz is for ubuntu os use it?

Thanks.

0 Kudos
Reply

2,393 Views
fdact
Contributor I

Thanks for your reply. I didn't know how to use IMX_MMCODEC_3.0.101_4.1.1_Bundle.tar.gz. Is there have any documentation for the use of this?

0 Kudos
Reply