System no response while  print out VPU blocking: timeout and rcu_sched_state

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

System no response while  print out VPU blocking: timeout and rcu_sched_state

2,879 次查看
fdact
Contributor I

I was play mp4 file, then a period of time found that there was no reaction to the system.This phenomenon is the probability of occurrence that need to play video a long time . I will upload the log . Can you give some advice?

 

 

Thanks.

Original Attachment has been moved to: systen_hang_up_paly_mp4.log.zip

标签 (1)
0 项奖励
回复
9 回复数

2,617 次查看
igorpadykov
NXP Employee
NXP Employee

this is kernel error, also android is based on linux.

~igor

0 项奖励
回复

2,617 次查看
igorpadykov
NXP Employee
NXP Employee

do you see red in my previous post from 05.06.2016 21:29

1.jpg

click on red with mouse.

0 项奖励
回复

2,617 次查看
fdact
Contributor I

HI igor,

    Our board uses android OS, but the document is for ubuntu OS.

0 项奖励
回复

2,615 次查看
igorpadykov
NXP Employee
NXP Employee

please refer to attached file

igor

0 项奖励
回复

2,615 次查看
fdact
Contributor I

Hi igorpadykon,

    I didn't find any attached file.

0 项奖励
回复

2,615 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ferdinand

seems you are using L3.0.35 with gpu lib 4.6.9, this is very old,

suggest to upgrade at least to L3.0.101_4.1.1 as it fixed many gpu bugs:

Board Support Packages (38)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite

Linux BSP Source Code Files (REV L3.0.101_4.1.1.)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,615 次查看
fdact
Contributor I

Hi igorpadykon,

    Now the problem is still not resolved, you have any way?

0 项奖励
回复

2,615 次查看
fdact
Contributor I

Hi igorpadykov,

   Files IMX_MMCODEC_3.0.101_4.1.1_Bundle.tar.gz is for ubuntu os use it?

Thanks.

0 项奖励
回复

2,615 次查看
fdact
Contributor I

Thanks for your reply. I didn't know how to use IMX_MMCODEC_3.0.101_4.1.1_Bundle.tar.gz. Is there have any documentation for the use of this?

0 项奖励
回复