Synchronous Dual Die NAND Flash DQS on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Synchronous Dual Die NAND Flash DQS on i.MX6

Jump to solution
961 Views
arnemaathuis
Contributor II

Hello,

I want to use a Micron Dual Die NAND Flash(MT29F64G08AEC) in synchronous mode on an DualLite i.MX6.

For both DQS lines i can't seem to find any info on how to connect these to NANDF_DQS(SD4_DAT0.alt2 on i.MX6)

Can i simply gang both DQS pin on the memory device(which i also did with the DQ-x Datalines and control logic interface ,except Chip Select)

Labels (2)
1 Solution
825 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arne

according to datasheet this nand is dual die with separate cs, dqs signals so

your understanding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
825 Views
arnemaathuis
Contributor II

Hello Igor,

thank you for this reply!

regards

0 Kudos
Reply
826 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arne

according to datasheet this nand is dual die with separate cs, dqs signals so

your understanding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply