Switching the formats in the camera fails to launch streaming in the iMX8Mplus platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Switching the formats in the camera fails to launch streaming in the iMX8Mplus platform

39,679 Views
koilarulraj
Contributor III

HI,

We have supported UYVY, SRGB10 formats from the camera and using iMX8MPlus kit for the evaluation.

After booting of the kit, if we first launch either UYVY or SRGB10, the stream works without any issues in the format. But when we try to switch between the format, the stream stops.

We have debugged the camera MIPI signals. It is correctly configuring with the required format and MIPI signal activity is proper in the camera.

But the iMX8Mplus platform not supporting the switching between the different formats. Is there any patches to resolve this issue?

We are using following kernel.
kernel : v6.1.55
Yocto : mickledore

Thanks.

0 Kudos
Reply
31 Replies

36,519 Views
koilarulraj
Contributor III

Hi @joanxie,

As per our previous discussion, I have added default supported formats (YUYV and RGB888) in the camera and tried the switching between the formats.

There are few kernel modifications required to properly set the required pixelformat in the sensor driver. Since the current iMX8MPlus kernel by default sets MEDIA_BUS_FMT_UYVY8_2X8 as the format code in the "drivers/staging/media/imx/imx8-isi-cap.c" file. Please find the kernel changes done in the attached patch.

The camera stream stops when switching between the formats same as before.

Case 1: Launching RGB888 first after the boot and then YUYV format.

root@imx8mp-var-dart:~/YUV_RGB_Binaries# v4l2-ctl -d 3 -v width=640,height=480,pixelformat='RGB3' --stream-mmap
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 113.68 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<^C
root@imx8mp-var-dart:~/YUV_RGB_Binaries#
root@imx8mp-var-dart:~/YUV_RGB_Binaries#
root@imx8mp-var-dart:~/YUV_RGB_Binaries# v4l2-ctl -d 3 -v width=640,height=480,pixelformat='YUYV' --stream-mmap

 

Case 2: Launching YUYV format first after the boot and then YUYV format.

root@imx8mp-var-dart:~# v4l2-ctl -d 3 -v width=1280,height=720,pixelformat='YUYV' --stream-mmap
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 75.40 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 75.40 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 75.40 fps
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<^C
root@imx8mp-var-dart:~#
root@imx8mp-var-dart:~# v4l2-ctl -d 3 -v width=640,height=480,pixelformat='RGB3' --stream-mmap

 

Kindly check this and let us know how to resolve this behavior?

Thanks.

36,677 Views
koilarulraj
Contributor III

Hi @joanxie ,

As per our testing, the camera is correctly configured with required format and the MIPI activity is proper.

We suspect on the platform couldn't sample the data properly during the format switch.

Can you please explain, what do you mean by default format and how to test it?

Thanks.

0 Kudos
Reply

36,656 Views
joanxie
NXP TechSupport
NXP TechSupport

the format you test is add by yourself, I mean you use the default format, not your own add format, you can use --list-formats to check all of format your camera support, then test the default one(not the raw10 you add), because I couldn't reproduce this on my side, I don't know if this issue is related to your camera driver or nxp bsp  source code, if could, could you test the camera the bsp support as default? to check if this issue is related to your bsp or your camera

0 Kudos
Reply

36,316 Views
koilarulraj
Contributor III

Hi @joanxie,

We tried to switch between (MEDIA_BUS_FMT_SGRBG10_1X10 & MEDIA_BUS_FMT_SGRBG8_1X8) With these two formats, we can able to properly switch between the streaming. But when we tried to switch to UYVY format,  the stream stops.

When debugging the drivers/staging/media/imx/imx8-mipi-csi2-sam.c driver code, In the mipi_csis_imx8mp_phy_reset function, UYVY related media bus formats are not handled.

Is this something related to the issue?

What is the PIXEL MODE value expected for the UYVY, SGRBG10, SGRBG8 formats?

Whether the imx8-mipi-csi2-sam.c driver is written to handle multiple format support?

Kindly let us know your thoughts to resolve this issue.

Thanks.

0 Kudos
Reply

36,177 Views
joanxie
NXP TechSupport
NXP TechSupport

"When debugging the drivers/staging/media/imx/imx8-mipi-csi2-sam.c driver code, In the mipi_csis_imx8mp_phy_reset function, UYVY related media bus formats are not handled."

> what do you mean media bus are not handled? do you  mind adding more debug information in this function and share more log? since I couldn't reproduce this issue and your logfile is too limit to find the root cause

0 Kudos
Reply

36,120 Views
koilarulraj
Contributor III

Hi @joanxie ,

Thanks for the reply. please find the reply below.

what do you mean media bus are not handled?

please find the attached image where in the "mipi_csis_imx8mp_phy_reset" function in the kernel platform driver(drivers/staging/media/imx/imx8-mipi-csi2-sam.c), the format "MEDIA_BUS_FMT_UYVY8_2X8" not handled. This phy_reset is getting called whenever we change the format & resolutions. And this function handles RAW8,10 and 12 format settings in the phy reset. So suspected whether this could be the reason.

do you mind adding more debug information in this function and share more log?

Please find the attached logs with more information.

Working_UUVY.txt - Log when streaming UYVY after the fresh boot.

NotWorking_UUVY.txt - Log after switching to other format and then retry UYVY.

Thanks.

0 Kudos
Reply

36,068 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems stuck here, couldn't get proper signal

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/media/common/videobuf2/videobuf2-core.c#L...

for more detailed information, refer to the function

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/include/linux/wait.h#L496

maybe you can add more debug information to trace, how about using gstreamer or unit test to change the format? still the same issue?

0 Kudos
Reply

35,459 Views
koilarulraj
Contributor III

Hi @joanxie,

Please find the replies below.

maybe you can add more debug information to trace,

Please find the attachments with more debug logs enabled from the kernel (CONFIG_DYNAMIC_DEBUG) and v4l2 core.

how about using gstreamer or unit test to change the format? still the same issue?

Yes. The format switch issue occurs even with Gstremer and unit test when changing the format.

 

The v4l2 layer not receiving the frame event. Seems like something failing at the CSI platform layer which blocks the system to properly receive the data. Kindly check the logs and share your suggestions.

Thanks.

0 Kudos
Reply

35,123 Views
koilarulraj
Contributor III

Hi @joanxie ,

Did you get chance to review the above logs with Gstreamer commands?

Suggestions from your end would be helpful to proceed with the debugging.

Thanks.

 

0 Kudos
Reply

34,150 Views
koilarulraj
Contributor III

Hi @joanxie,

Any inputs on this topic. We would really appreciate any debugging technique to gather more details on the issue.

Thanks.

0 Kudos
Reply

33,863 Views
joanxie
NXP TechSupport
NXP TechSupport

sorry I was handling a urgent case before, could you tell me what do the each logfiles stand for? they all work under yuv format, right? 

0 Kudos
Reply

32,673 Views
koilarulraj
Contributor III

Hi @joanxie,

Sure. Please find the explanation for each log file.

working_uyvy_log_with_gstreamer.txt

     a) Logs when streaming UYVY format after fresh boot.

not_working_jpeg_format_log_with_gstreamer.txt

     a) Log when switching the stream to MJPG format from UYVY format.

     b) Now stream blocks without any error in the dmesg. And no frame ready interrupt received in the platform drivers.

not_working_uyvy_format_after_switch_from_jpeg_format_log_with_gstreamer.txt

     a) During the not working condition, stop the MJPG stream and again tried launching UYVY format. There is no stream received in the platform.

The stream fails when switch from or switch to UYVY format in the iMX8Mplus platform. Looking forward to your response to resolve this issue.

Thanks.  

 

0 Kudos
Reply

32,575 Views
joanxie
NXP TechSupport
NXP TechSupport

I remembered you couldn't switch between raw data with yuv data, now you test between yuv with mjpeg? anyway, I checked your not_working_jpeg_format_log_with_gstreamer, CSIS_DPHYSTATUS[20]: 0x00000001, which means the clock is under stop state, you need check if this bit is always be set in stop state, and when you capture, try to use oscilloscope to check if the camera work correctly after you switch

0 Kudos
Reply

32,073 Views
koilarulraj
Contributor III

Hi @joanxie,

Sorry for the late reply. Held up with other tasks.

Yes. In our setup we take  UYVY, MJPG and RAW10 formats from the camera. MJPEG format is taken as fixed size. (ie) (width x height).

After switching the format, we confirmed the frame activity in both ISP logs from the camera and by taking probe in the MIPI signals. The data activity is proper in the camera side.

As per your input,  CSIS_DPHY control register values are same in both working and not working condition as given below.

From working_uyvy_log_with_gstreamer.txt:
[ 801.447120] mxc-mipi-csi2.0: CSIS_DPHYCTRL[24]: 0x1780001f
[ 801.447124] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_L[30]: 0x000001f4
[ 801.447128] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_H[34]: 0x00000000
[ 801.447133] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_L[38]: 0x00000000
[ 801.447137] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_H[3c]: 0x00000000

From not_working_jpeg_format_log_with_gstreamer:

[ 963.056933] mxc-mipi-csi2.0: CSIS_DPHYCTRL[24]: 0x1780001f
[ 963.056937] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_L[30]: 0x000001f4
[ 963.056942] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_H[34]: 0x00000000
[ 963.056947] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_L[38]: 0x00000000
[ 963.056951] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_H[3c]: 0x00000000

So, the platform driver also seems initializing the lanes and clock to the required working state.

Is there any way we can force the DPHY to reenable state or reset state to avoid this clock stop status error in the platform drivers when switching between UYVY to other formats and vice versa?

Thanks.

Tags (1)
0 Kudos
Reply

32,056 Views
joanxie
NXP TechSupport
NXP TechSupport

Is there any way we can force the DPHY to reenable state or reset state to avoid this clock stop status error in the platform drivers when switching between UYVY to other formats and vice versa?

> as I mentioned before, pls check the bit20 of  CSIS_DPHYSTATUS, if this bit is always be set stop status. refer to the application note, the reset steps are:

The reset and initialization procedure for the i.MX 8MM/i.MX 8MN/i.MX 8MP MIPI CSI-2 Rx subsystem is as
follows:
1. Assert SW reset. It is deasserted automatically after the software reset is done.
2. Configure DPHY:
a. DPHY slave control (register MIPI_CSIx_DPHY_SLAVE_CTRL_LOW)
b. DPHY master and slave control (register MIPI_CSIx_DPHY_MASTER_SLAVE_CTRL_LOW/HIGH)
c. DPHY common control, such as enabling data lane 0/1/2/3, setting HS settle timer
(MIPI_CSIx_DPHY_COMMON_CTRL)
3. Configure CSIS:
a. Interrupt mask (register MIPI_CSIx_INTERRUPT_MASK_0)
b. CAM/ISP interface settings, such as image data type, vertical/horizontal image resolution (register
MIPI_CSIx_ISP_CONFIG0, MIPI_CSIx_ISP_RESOLUTION0, and MIPI_CSIx_ISP_SYNC0)
c. CSIS clock control (register MIPI_CSIx_CSIS_CLOCK_CTRL)
d. CSIS common control, such as the number of data lanes (register MIPI_CSIx_CSIS_COMMON_CTRL)
4. Configure Gasket (only for i.MX 8 MN and i.MX 8MP):
a. Gasket control, such as data type, interlace mode (register GPR_GASKET_x_CTRL)

b. Gasket video size setting (register GPR_GASKET_x_HSIZE and GPR_GASKET_x_VSIZE)

0 Kudos
Reply

36,244 Views
koilarulraj
Contributor III

Hi @joanxie,

As per the ISI_OUT_FMT definition in the TRM (image in the attachment), YUYV format is stored interleaved packed bytes. Whereas RAW formats are stored word type. Will this cause any problem when switching between the formats in memory level?. Because, we observe issues only when switching between YUYV format.

We aware that, using ISP interface switching is working with os08a20 camera. But is there any reference for cameras which only use the ISI interface to properly switch between the formats.

Looking forward to your response.

0 Kudos
Reply

36,675 Views
koilarulraj
Contributor III

Hi @joanxie,

We are checking with the following BSP. But please note that we observe the same behavior even in the 5.10 and 5.15 kernel version.

BSP Details:
Kernel - v6.1.55.

Yocto - Mickledore

 

Please find our additional kernel changes to support UYVY and BA10 format in the attachment (ar1335_imx8mplus_kernel.patch).

Kindly share your suggestion to resolve this issue.

Thanks.

0 Kudos
Reply

36,664 Views
joanxie
NXP TechSupport
NXP TechSupport

could you reproduce this issue with default format? I don't have this camera to reproduce this, I need to know if this issue is related to the camera or not, could you test the default format again?

0 Kudos
Reply

36,698 Views
CunningJaguar
Contributor I

It sounds like you're troubleshooting an issue with the board’s video output. When you boot it up and test 'UYVY,' you want to make sure everything is functioning correctly before moving on to capturing in raw10 format. If you're experiencing the same problem with the raw10 capture as with the UYVY test, it could indicate a deeper issue, possibly with the board’s hardware or the way it's processing those formats. Have you checked the connections and ensured that all drivers and firmware are up to date? It might also help to look at any error messages or logs that could give more insight into what’s going wrong.

0 Kudos
Reply

36,699 Views
koilarulraj
Contributor III

Hi @joanxie,

Yes. After the bootup if we first test the UYVY format. It works properly as given below.

# v4l2-ctl -d 3 -v width=4192,height=3120,pixelformat='UYVY' --stream-mmap
[ 47.987726] streamdb[0]=0, mode=4
[ 47.987743] streamdb[1]=1, mode=4
[ 47.991104] streamdb[2]=2, mode=4
[ 47.994461] streamdb[3]=3, mode=4
[ 47.997801] streamdb[4]=4, mode=4
[ 48.001133] Index = 0x0004 , format = 0x59565955, width = 4192, height = 3120, frate num = 13
[ 48.066036] bypass csc
[ 48.068416] input fmt YUV4
[ 48.071127] output fmt UYVY
<<<<<<<<<<<<<<< 13.00 fps
<<<<<<<<<<<<< 13.00 fps
<<<<<<<<<<<<< 13.00 fps
<<<<<<<<<<<<< 13.00 fps
<<<<<<<<<<<<< 13.00 fps
<<<<^C
root@ucm-imx8m-plus:~#

After that, if we try RAW10 the stream not working as given below.

# v4l2-ctl -d 3 -v width=4208,height=3124,pixelformat='BA10' --stream-mmap
[ 79.250902] streamdb[0]=0, mode=8
[ 79.250920] streamdb[1]=1, mode=8
[ 79.254250] streamdb[2]=2, mode=8
[ 79.257590] streamdb[3]=3, mode=8
[ 79.260929] streamdb[4]=4, mode=8
[ 79.264264] streamdb[5]=5, mode=8
[ 79.267595] streamdb[6]=6, mode=8
[ 79.270923] streamdb[7]=7, mode=8
[ 79.274242] streamdb[8]=8, mode=8
[ 79.277571] Index = 0x0008 , format = 0x30314142, width = 4208, height = 3124, frate num = 20
[ 79.330466] input fmt BA10
[ 79.333186] output fmt BA10

 

Basically, only one format is working in the iMX8MPlus. Switching between the format is not working. Is there any reason for this issue and any patches available for this issue?

From our debugging, all the configuration for the format in the platform drivers are correctly setting as in the working case. But system couldn't receive the frames after the format switching.

Thanks.

0 Kudos
Reply