We are considering using iMX6 for one of our projects that needs to drive a 1280x800 LCD.
This product doesn't need a lot of CPU power, and it doesn't really need GPU.
But seems like some of the lower-end iMX6 (like the UUL, UL) CPU can only support up to 1388x768.
Can iMX6UUL or UL reconfigure to support 1280x800 LCD resolution?
Or what is the lowest-end iMX6 that can support 1280x800 LCD via LVDS/MIPI interface?