Is there available any camera modules supported by i.MX7 Sabre board?
Alternatively is there schematics for a cable/converter to connect a generic MIPI camera like OV5640 to Sabre board CSI flat cable connector.
Solved! Go to Solution.
Hi Ari
the camera module used for the imx7SABRE board is from Truly and
can be purchased from Boundary Devices
https://boundarydevices.com/product/nit6x_5mp_mipi/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ari, I came across e-con Systems e-CAM80_IMX7, 8MP camera MIPI camera board for iMX7 Sabre board iMX7 MIPI Camera Interface | 8MP iMX7 Camera
I just received Sabre board and the CSI connector is not a flat cable connector. Instead there is board2board connector.
Have you changed the connector as in the images and in schema that I have the connector is different.
Anyway do you have a camera that can be connected to this connector or an adapter for MIPI camera?
Hi Ari
the camera module used for the imx7SABRE board is from Truly and
can be purchased from Boundary Devices
https://boundarydevices.com/product/nit6x_5mp_mipi/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks, ordered one.
Is there already support for this camera in Sabre board Linux Kernel?
yes it is supported in Linux 4.1.15_1.2.0