Supported Camera Sensor for i.MX6 Series board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported Camera Sensor for i.MX6 Series board.

678 Views
kailas_kharse
Contributor IV

Hello Team,

I want to know what all types of Camera sensors are supported in i.Mx6 Dual / Quad Series of SoC.

I am planning to use one of the listed camera sensors. Can you list which one will directly support/support with minimal changes?

DescriptionPart NumberResolution
Full camera + LED + ISPV31105L Series1920x1080
Full camera + LED + ISPMD-V22605L-741200x1080
Full camera + LED + ISPB21105 Series1280x720
   
Sensor + ISP onlyB164B03 SERIES1280x720
Sensor + ISP onlyB31105 SERIES1920x1080
Sensor + ISP onlyB36305 SERIES2592x1944
   
 OV56402592x1944
 OH02A101920x1080
 OH08A404024x2180

 

Immediate help will be appreciated.

 

Thanks & Regards,
Kailas Kharse

0 Kudos
Reply
3 Replies

669 Views
joanxie
NXP TechSupport
NXP TechSupport

current bsp supports ov5640 and ov5642 for imx6q as default

0 Kudos
Reply

648 Views
kailas_kharse
Contributor IV

Hello Joanxie,

Our customer is insisting to use either of the camera listed, Can you please inform can we used this camera directly?

Video Format: MJPEG / YUV
Interface: USB 2.0 (Compliant with USB Video Class 1.1 Standard)
Frame Rate: 15~30 fps

 

DescriptionPart NumberResolutionODPixel SizeInterfaceFPS 
Full camera + LED + ISPV31105L Series1920x10805.4 to 7.81.4USB15-30 
Full camera + LED + ISPMD-V22605L-741200x10805.41.4USB30 
Full camera + LED + ISPB21105 Series1280x7205.51.4USB30 
        
Sensor + ISP onlyB164B03 SERIES1280x7203.241.12USB30-60 
Sensor + ISP onlyB31105 SERIES1920x10804.91.4USB30 
Sensor + ISP onlyB36305 SERIES2592x19445 USB24 
0 Kudos
Reply

639 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately these camera didn't be tested officially, if customer use usb camera, the bsp should support them as default, for performance, maybe you can check the link

"https://community.nxp.com/t5/i-MX-Processors/VPU-performance-CSI-2-MIPI-camera-vs-USB-camera/m-p/293..."

0 Kudos
Reply