Support exFAT filing system on SD card.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Support exFAT filing system on SD card.

829 次查看
divyeshmarne0
Contributor III

Hi Team,

  1. We have imx8mm device with Android 11 code. Added support for SD card in fstab entry.
  2. Could you please help here to support the exFat filing system on SD cards.

also we need following path to locate external storage (SDCARD) in adb shell:

  1. /sdcard/

Currently it is points to the internal memory which is android file system.

We need /sdcard path as a /sdcard/<Sdcard_name_byUser>

 

Thanks

Divyesh

 

标签 (1)
0 项奖励
3 回复数

788 次查看
divyeshmarne0
Contributor III

Hi @joanxie ,

We have added support for exfat in Android 11 code base. Now exfat formatted SDcard is supporting.

But we are not able to create folder in /sdcard folder. We need External sdcard points to the /sdcard/ClubCar directory. But in current implementation it is pointing to internal storage of device. need to change path to point External sdcard. Could you please help here ?

 

Thanks 

0 项奖励

798 次查看
divyeshmarne0
Contributor III

Hi @joanxie ,

I tried to format SDcard with exfat and it is working through adb shell :

evk_8mm:/ # mkfs.exfat /dev/block/mmcblk1p1
mkexfatfs 1.3.0
Creating... done.
Flushing... done.
File system created successfully.

After executing these commands, I can see type=exfat.

BUT I need default format exfat without any commands through adb shell...

 

0 项奖励

806 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励