Support exFAT filing system on SD card.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support exFAT filing system on SD card.

832 Views
divyeshmarne0
Contributor III

Hi Team,

  1. We have imx8mm device with Android 11 code. Added support for SD card in fstab entry.
  2. Could you please help here to support the exFat filing system on SD cards.

also we need following path to locate external storage (SDCARD) in adb shell:

  1. /sdcard/

Currently it is points to the internal memory which is android file system.

We need /sdcard path as a /sdcard/<Sdcard_name_byUser>

 

Thanks

Divyesh

 

Labels (1)
0 Kudos
3 Replies

791 Views
divyeshmarne0
Contributor III

Hi @joanxie ,

We have added support for exfat in Android 11 code base. Now exfat formatted SDcard is supporting.

But we are not able to create folder in /sdcard folder. We need External sdcard points to the /sdcard/ClubCar directory. But in current implementation it is pointing to internal storage of device. need to change path to point External sdcard. Could you please help here ?

 

Thanks 

0 Kudos

801 Views
divyeshmarne0
Contributor III

Hi @joanxie ,

I tried to format SDcard with exfat and it is working through adb shell :

evk_8mm:/ # mkfs.exfat /dev/block/mmcblk1p1
mkexfatfs 1.3.0
Creating... done.
Flushing... done.
File system created successfully.

After executing these commands, I can see type=exfat.

BUT I need default format exfat without any commands through adb shell...

 

0 Kudos

809 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos